Other Parts Discussed in Thread: TMUX1308,
请问下对于TMUX1308来说,如果VDD是5V供电,D端输入的是否可以是1.8V电平的方波信号,此时是否需要在S端加上Pull High,若不加Pull high ,S端是否可以正常输出0-1.8V的信号;若VDD为1.8V时,上述情况的信号是否能够正常传输,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问下对于TMUX1308来说,如果VDD是5V供电,D端输入的是否可以是1.8V电平的方波信号,此时是否需要在S端加上Pull High,若不加Pull high ,S端是否可以正常输出0-1.8V的信号;若VDD为1.8V时,上述情况的信号是否能够正常传输,谢谢!
您好,
TMUX1308-Q1 可在源极 (Sx) 和漏极 (Dx) 引脚上支持从 GND 到 VDD 范围的双向模拟和数字信号,因此,在VDD为5V或1.8V时,都可以传输0-1.8V的信号。但输出会由于MUX导通阻抗、漏电流、信号频率(带宽导致的衰减)产生一定的误差,下面链接帖子解释的很详细:
注意信号带宽:

“在S端加上Pull High”是指在输出端接上拉电阻至电源吗?这里不需要的。