This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6121: 使能双通道开关,两个不同通道之间是否会相互影响。能否一个通道输出负电压,一个开关输出正电压。

Part Number: TMUX6121
Other Parts Discussed in Thread: TPS22810, LM3880, TMUX6219

您好!我最经在使用TMUX6121设计使能控制上电时序单路。TMUX6121作为使能控制开关,在使能信号到达时,同时导通,然后一路输出正电压,一路输出负电压。目前的问题是,正电压本来应该是+12V,但是现在的输出值只有+5V。两个通道是不是会相互影响,不能同时输出正电压和负电压。

下面是我的上电时序电路,使用LM3880按时序产生使能信号,然后控制不同的使能开关导通来完成电源时序控制,U4为TMUX6121,U3和U5是TPS22810,请帮我看一下设计方案是否有问题。