Part Number: TMUX4052
Hi :
你好!
TMUX4052这个开关能不能切换RS485信号,如果不能,帮忙描述一下为什么不能,再帮忙推荐一个型号,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以,RS485的共模电压范围-7V~12V,TUMUX4052可以双电源供电,VDD电压范围5V~24V,VSS为-15V~0V范围,并且VDD和VSS可以在任意电压范围只要保证VDD-VSS在5V~24V范围内即可。所以满足485的电压要求,带宽的话如下,不知您的485信号速率多大?只要带宽和IO电压符合,就没有问题。


RS485切换有没有电流方面的要求?如果TUMUX4052的导通电阻太大,是不是会影响RS485的通信距离 ?
485接收端的IO电流我查了一款收发器的电气参数,sink 和source电流为4mA,当然开关的导通电阻越小,流过开关的电流在导通电阻上形成的压降越小。

但是不会超过-7V~12V的电压范围。 通信距离主要是和data rate有关的,通信距离和data rate成反比。