This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4067: 关于多片CD74HC4067 MUX芯片级联问题

Part Number: CD74HC4067


您好!我现在要用到4个16选1  MUX开关芯片,但是MCU的管脚有限,能否通过将4个MUX芯片的4位地址线S0/S1/S2/S3连接再一起接到MCU的IO口,再通过EN/脚来依次片选4个芯片?CD74HC4067手册里面我没有看到EN使能关闭条件下,S0/S1/S2/S3具体是什么状态?是高阻态吗?

如果可以按照上述接法级联的话,四路MUX芯片的使能也可以同时打开吗?

  • 您好,

    看下面截图是 CD74HC4067的真值表,S0/S1/S2/S3是输入管脚,在E管脚高电平时,S0/S1/S2/S3的状态不管是什么状态,是没有通道被选择输出的:

    如果可以按照上述接法级联的话,四路MUX芯片的使能也可以同时打开吗?

    看您上面描述,这应该是四路MUX芯片并联?四路MUX芯片同时使能的话,相当于四路MUX芯片的同一编号的通道同时选择输出。这是可行的。