Part Number: SN74CBTLV3125
Dear all,
如标题所示,SN74CBTLV3125的标题页面标注BW为200MHz,但是在规格书中并未查到对应参数,请问200MHz这个值是计算得到的还是实际测试的?是否具有实际的参考价值?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74CBTLV3125
Dear all,
如标题所示,SN74CBTLV3125的标题页面标注BW为200MHz,但是在规格书中并未查到对应参数,请问200MHz这个值是计算得到的还是实际测试的?是否具有实际的参考价值?

您好,数据手册中确实没有给出支持的带宽参数。
通常我们可以根据tpd这个传输延迟估算下能支持的data rate,估算方法就是最大传输延迟的倒数。
可以看到SN74CBTLV3125的传输 延迟tpd在VCC=2.5V时,tpd=0.15ns。VCC=3.3V时,tpd=0.25ns。
那么根据最大0.25ns去计算,1/0.25ns=400Mbps=200Mhz.和主页上描述的是相符的。
那么我们在使用的时候尽量留有更多的余量,比如说支持50Mhz的信号是没问题的。
如果这些逻辑器件的数据手册没有给出具体的带宽参数,我们可以用传输延迟来进行估算,从而评估是否满足应用。