This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219: 请教关于此开关的一些问题

Part Number: TMUX6219
Other Parts Discussed in Thread: TS5MP646

最近在测试TMUX6219 SPDT 这个开关的时候发现几个问题,请帮忙解答一下,测试条件 VDD +15V,VSS-15V ,EN (H) 5V EN (L) 0V SEL (H) 5V EN (L) 0V 

1、TMUX6219 当输入1K 2V VPP的正弦波信号时,提供EN 信号和SEL 信号,使用示波器观察发现输出信号畸变为三角波信号,同时赋值有降低,麻烦分析下可能的原因

2、请问TMUX6219支不支持级联?如果输入模拟信号经过了4个TMUX6219,出来的信号的指标会下降成什么程度有没有一个大概的指标

谢谢