Part Number: TS3L301
我有一个项目,很简单:使用MCU控制网络A口和B口导通,或者A与C口通。原先使用MAX的MAX4890ETJ+T完成了设计。控制导通时,双掷开关的两侧的电阻确实很小。
换成TI的TS3L301芯片(主要考虑封装问题),彻底翻车了,控制导通后,双掷开关两侧的电阻确实不是无穷大,但是也不是手册中的很小的阻值,而是几K欧,还变化的。
有没有谁能告知这是真么回事儿?
要怎么做才行?
设计RJ45网口A-》TS3l301-》RJ45网口B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3L301
我有一个项目,很简单:使用MCU控制网络A口和B口导通,或者A与C口通。原先使用MAX的MAX4890ETJ+T完成了设计。控制导通时,双掷开关的两侧的电阻确实很小。
换成TI的TS3L301芯片(主要考虑封装问题),彻底翻车了,控制导通后,双掷开关两侧的电阻确实不是无穷大,但是也不是手册中的很小的阻值,而是几K欧,还变化的。
有没有谁能告知这是真么回事儿?
要怎么做才行?
设计RJ45网口A-》TS3l301-》RJ45网口B
您好,
我大体对比了下两产品,TS3L301的-3dB带宽是900MHZ,而MAX4890ETJ是1000MHZ,看下是否带宽不够造成的?

TS3L301具体输出信号是怎样的?TS3L301的Con电容也大一些,我想看下是什么因素导致TS3L301 不能正常工作?
TI没有找到能替换MAX4890ETJ+T的芯片