This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN3257-Q1: Does the floating pin will damage the device

Part Number: SN3257-Q1


Hello team,

We used two devices for the signal switching,and the pin 14(S4A) of one of them is not used.

After two months,we noticed that the unused one is damaged,the pins(S4A,S4B) are short-circuited to ground.

We would like to know if there is a connection between the two things.

In the 8.4 of the data sheet,I saw that "Unused signal path inputs (SxA, SxB, or Dx) should be connected to GND. "

But I cant find the more description about this.

Best,

Richard