This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于多路复用器TMUX1511的相关问题

Other Parts Discussed in Thread: TMUX1511

你好,我打算利用一个八选一多路复用器去选通电阻,该电阻是用于选通我仪表放大器的增益电阻的。电源正负供电为±12V,用逻辑高低电平去控制通断。

我用的是两个TMUX1511构成8通道,当我和仪表放大器AD8429连接后,不管我是否给SELx逻辑信号,芯片的所有通道总是全导通(比如我测试时用信号发生器输入到仪表放大器的信号为1V@1KHz的正弦信号,示波器上显示的波形为饱和,但是此时理论上导通的引脚应为D1,SEL1通道设的增益为10倍,理论上在示波器显示应为10V,应该未到饱和电压的)

我单独测试仪表放大器AD8429是没有问题的。因此怀疑是否多路复用器的问题。高电平给的是3.3V,低电平给的是0V。

我也单独测试过多路复用器,当我给SEL1给高电平3.3V时,测试芯片2 3引脚导通,5 6 引脚也是导通的。理论上5 6引脚不应该导通才对。

原理图中的RG1和RG2是连接到仪表放大器的增益引脚两端的。