Part Number: TMUX136
上述图片电路的电流异常大,且接上tmux136是使得5v的电源变成1.4v。请查阅电路是否有问题。
part b的电路测试的电压在-0.05v,part b是通过一个隔直电容接入到part b,part a的电压也是在0v,part a是通过一个100欧姆 的电阻接入到比较器的同相输入端,com端是接的sma外部未接入电路,com端处于悬空
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
虽然 TMUX136最大耐压到5.5V,但是推荐的供电范围是最大到4.8V,因此不建议使用超出推荐范围外的电压供电,因为这不能保证其datasheet 中列出的电气性能。


另外模拟输入电压范围是0 ~ 3.6V,不能输入负的电压。

part b的电路测试的电压在-0.05v,part b是通过一个隔直电容接入到part b
有对隔直电容充电吗?
您修改 TMUX136 供电电压到推荐的供电范围,然后2channel 输入都接地,TMUX136 工作正常吗?还会拉下供电电压吗?