Part Number: TS5A23159
假设V+ pin接3.3V,GND pin接系统地,IN1接系统地,COM1上输入-0.3V,那么在NC1 pin上的电压是-0.3V吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS5A23159
假设V+ pin接3.3V,GND pin接系统地,IN1接系统地,COM1上输入-0.3V,那么在NC1 pin上的电压是-0.3V吗
您好,
-0.3V不在推荐的输入范围内,因此不能保证其电气性能。

如果您需要 负电压传输,建议选用双电压供电的多路开关,这样可以输入负压,不知道您对多路开关有什么要求,您是需要2:1 SPDT是吗?通道数、带宽、Ron、供电电压或输入信号幅值、温度范围等参数有什么要求,或您自己也可以在下面链接选型:
https://www.ti.com.cn/zh-cn/switches-multiplexers/analog/products.html#1143=2%3A1%20SPDT&
如果我将V+ pin接3.3V,GND pin接-1V,这样的话可以输入并传输负电压吗
应该可以的,但是控制管脚INx的高和低电平电压也随之改变,因为参考点电压变了。


从上面截图中可以看出,不管VCC=5V还是3.3V,INx低电平定义范围都是0~0.8V,若使用-1V,3.3V供电,INx 低电平应该在-1V ~ -0.2V 之间,所以这个电压也需要额外的电源产生。
INx 高电平范围比较广,您可以使用供电电压3.3V去控制。