我向AHD视频信号二选用一,不知道用什么开关芯片,麻烦tiFAE推荐下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,AHD视频信号的带宽以及IO电压是多少?然后根据IO电压以及能支持的带宽,方便更好的帮您选型。
https://www.ti.com/product/TMUX136
比如您可以先看下TMUX136这款2:1 开关是否满足您的需求。
您好,
13.5M 控制电平3.3V
TMUX136可以满足要求。带宽和IO电压符合基本上就是没问题的。
另外,注意下AHD信号是差分信号吧?TMUX136是符合差分信号应用的2选1架构。