CODECOMPOSER: Improve Layout Flexibility in CCS21 (Theia) – Enable Drag-and-Drop for Debug Sub-Windows

Part Number: CODECOMPOSER

Hi there,

I am writing to submit a feature request regarding the UI layout flexibility in Code Composer Studio v21 (Theia-based).

Currently, in CCS21, sub-windows inside the DEBUG view—such as Threads, Call Stack, Variables, and Expressions/Watch—are constrained and cannot be freely dragged and dropped into different screen regions. This is a significant regression from the Eclipse-based CCS12, which allowed complete freedom in customizing the workspace layout.Furthermore, CCS21 splits layouts into distinct "Edit" and "Debug" perspectives. My goal is to maximize the visibility of debugging information when in the Debug perspective, rather than having everything crammed into a single, crowded window pane. However, once I exit the debugging session, I need the layout to automatically restore to the normal "Edit" view so it does not interfere with code writing.To be completely honest, the current limitation of this rigid layout is a major reason why I, and many other users, am hesitant to migrate from CCS12 to the new Theia-based versions.

Kind regards

image.png