This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6000 8.3.8 编译器在编译使用C++14 STL库的OpenMP工程时报内部错误

当编译只有一个main.cpp文件的OpenMP工程时,如果代码中使用的STL库,编译器会报内部错误,语言标准为C++14,器件为c6678。main.cpp代码如下:

#include <vector>

struct ABC{
    float *data;
}

void test_fxn(const std::vector<ABC>& obj)
{
    float * data=obj[0].data;
}

报如下错误:

**** Build of configuration Debug for project test ****

"C:\\ti\\ccs930\\ccs\\utils\\bin\\gmake" -k -j 64 all -O

Building file: "../main.cpp"
Invoking: C6000 Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c6000_8.3.8/bin/cl6x" -mv6600 --include_path="C:/Users/YuHaoxin/Documents/CCS_Workspace/test" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c6000_8.3.8/include" -g --c99 --c++14 --diag_warning=225 --diag_wrap=off --display_error_number --multithread --openmp --preproc_with_compile --preproc_dependency="main.d_raw" --cmd_file="C:/Users/YuHaoxin/Documents/CCS_Workspace/cfg/Debug/configPkg/compiler.opt" "../main.cpp"

>> Compilation failure
subdir_rules.mk:9: recipe for target 'main.obj' failed

INTERNAL ERROR: C:\ti\ccs930\ccs\tools\compiler\ti-cgt-c6000_8.3.8\bin\acpia6x.exe experienced a segmentation fault
while processing function (unknown or file scope) file ../main.cpp line 9

This is caused by a defect in the TI EABI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".

We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment

gmake: *** [main.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

编译选项为:

-mv6600 --include_path="C:/Users/YuHaoxin/Documents/CCS_Workspace/test" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c6000_8.3.8/include" -g --c99 --c++14 --diag_warning=225 --diag_wrap=off --display_error_number --multithread --openmp
如果去除"--openmp"选项,则编译通过。

我的项目需要同时用的Openmp和C++14的STL,请问该如何解决这个问题?