This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS3.3 版本与其他版本的区别 cl2000 asm2000差异

Part Number: TMS320F2812


TI 工程师

          当前项目是基于F2812,需要把很久远的一个程序脱离ccs编译器,只利用编译环境来编译。原始程序是ccs3.3版本下实现的。

问题:

1. 当前64位WIN10无法安装3.3版本,不能真正编译,看实际编译过程的;

2. 原始程序用make方式编译时,tools选择10.4的ti-cgt-c2000_20.2.5.LTS\bin 勉强可以生成obj 文件,但切换成原始3.3的编译器文件cgtools\bin 就会出现已下警报

makefile:320: recipe for target '..\app\rfapp.obj' failed
make: *** [..\app\rfapp.obj] Error -1073741511

想了解ccs3.3 和10.4 版本的编译过程是如何的,有什么技术文档可以参考。

cl2000 asm2000这些编译器都增加了那些功能,

哪里可以下载3.3版本的安装程序,特别想看TI例子里的makefile是怎样设置的,对于.c .asm文件的编译过程。