Other Parts Discussed in Thread: AWR1642
这个函数是AWR1642的SDK2.0中cli.c第216行给出的代码,我不太明白他有什么用,我贴出代码以供参考
static void CLI_task(UArg arg0, UArg arg1)
{
uint8_t cmdString[256];
char* tokenizedArgs[CLI_MAX_ARGS];
char* ptrCLICommand;
char delimitter[] = " \r\n";
uint32_t argIndex;
CLI_CmdTableEntry* ptrCLICommandEntry;
int32_t cliStatus;
uint32_t index;
/* Do we have a banner to be displayed? */
if (gCLI.cfg.cliBanner != NULL)
{
/* YES: Display the banner */
CLI_write (gCLI.cfg.cliBanner);
}
/* Loop around forever: */
while (1)
{
/* Demo Prompt: */
CLI_write (gCLI.cfg.cliPrompt);
/* Reset the command string: */
memset ((void *)&cmdString[0], 0, sizeof(cmdString));
/* Read the command message from the UART: */
UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));
/* Reset all the tokenized arguments: */
memset ((void *)&tokenizedArgs, 0, sizeof(tokenizedArgs));
argIndex = 0;
ptrCLICommand = (char*)&cmdString[0];
/* comment lines found - ignore the whole line*/
if (cmdString[0]=='%') {
CLI_write ("Skipped\n");
continue;
}
/* Set the CLI status: */
cliStatus = -1;
/* The command has been entered we now tokenize the command message */
while (1)
{
/* Tokenize the arguments: */
tokenizedArgs[argIndex] = strtok(ptrCLICommand, delimitter);
if (tokenizedArgs[argIndex] == NULL)
break;
/* Increment the argument index: */
argIndex++;
if (argIndex >= CLI_MAX_ARGS)
break;
/* Reset the command string */
ptrCLICommand = NULL;
}
/* Were we able to tokenize the CLI command? */
if (argIndex == 0)
continue;
/* Cycle through all the registered CLI commands: */
for (index = 0; index < gCLI.numCLICommands; index++)
{
ptrCLICommandEntry = &gCLI.cfg.tableEntry[index];
/* Do we have a match? */
if (strcmp(ptrCLICommandEntry->cmd, tokenizedArgs[0]) == 0)
{
/* YES: Pass this to the CLI registered function */
cliStatus = ptrCLICommandEntry->cmdHandlerFxn (argIndex, tokenizedArgs);
if (cliStatus == 0)
{
CLI_write ("Done\n");
}
else
{
CLI_write ("Error %d\n", cliStatus);
}
break;
}
}
/* Did we get a matching CLI command? */
if (index == gCLI.numCLICommands)
{
/* NO matching command found. Is the mmWave extension enabled? */
if (gCLI.cfg.enableMMWaveExtension == 1U)
{
/* Yes: Pass this to the mmWave extension handler */
cliStatus = CLI_MMWaveExtensionHandler (argIndex, tokenizedArgs);
}
/* Was the CLI command found? */
if (cliStatus == -1)
{
/* No: The command was still not found */
CLI_write ("'%s' is not recognized as a CLI command\n", tokenizedArgs[0]);
}
}
}
}