Other Parts Discussed in Thread: AWR1843, SYSBIOS
平台:64位Windows系统。
安装的CCS版本为10.1.0
安装的mmwave SDK软件版本为mmwave_sdk_03_04_00_03。
进行毫米波雷达工程的创建(目标板为AWR1843),新建CCS工程中,命名MCU(Cortex R4F架构)对应文件名为m0329_mss,命名DSP(型号为TMS320C674x)对应文件名为m0329_dss。CCS工程新建完成后(过程没有问题,SYS/BIOS等mmwave SDK对应的库都已配置安装),进行编译,结果出现如下错误。
CCS10.1.0新建CCS工程后,还未进行任何配置或操作,编译dss和mss时都报错。
dss报错是:warning#10247-D:creating output section “.text”without a SECTIONS specification以及error #10234-D:unresolved symbols remain和error #10010:during linking;.out文件not built等错误,怎么解决?

以dss为例,Error和Warning描述如下:

10个Warning:
warning #10247-D: creating output section ".text" without a SECTIONS specification。
...
细看信息,这10个Warning都与SECTION有关,是CMD文件的问题吗?需要对CMD文件怎么操作或者设置?请贵人帮解答一下,谢谢。
而报错信息中的7个error中,报错信息有4条如下:
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "m0329_dss.out" not built
gmake[1]: *** [m0329_dss.out] Error 1
gmake: *** [all] Error 2
这些又是什么意思?如何解决?请教,谢谢!