This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ21701: 我在使用该款DC-DC电源芯片时我设置其输出为6V,输出电流最大只能到0.84A

Part Number: LMZ21701


我在使用LMZ21701SILR做直流电源转换,设置芯片到最大输出6V,使用直流程控电源提供12V电源,输出接电子负载仪器,使用电子负载仪拉负载,最多只能拉到输出0.84A,但是芯片标称输出1A,请问这正常吗?会是什么原因造成的呢?

原理图如下: