This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600-DESIGN-CALC: UCC25600, Simulation Design Verification

Part Number: UCC25600-DESIGN-CALC
Other Parts Discussed in Thread: UCC25600, UCC27200

I am designing a full-bridge LLC resonant converter using UCC25600 with UCC27200 gate driver to drive the full bridge. For this DC-DC converter, the specifications are Vin=38-42V, Vout=24V, Pout=500W, and I have selected Frequency=100KHz. I have used the document SLUP263 for my understanding and simulated the circuit in PSpice for TI. I want to send my design files, so for that, if an email address is shared, I will then send the files. The simulation is taking a lot of time, and I also want an expert opinion on the design and also all the component values that I have used before making the hardware.