This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678: 出现ccs报错 error 503 连不上target

Part Number: TMDSEVM6678


IcePick_D: Error connecting to the target: (Error -503 @ 0x0) The user selected phase-one auto-range frequency failed the scan-path test. The utility or debugger requested the JTAG controller and cable, that generate the JTAG clock, to use a user selected feature or algorithm. The built-in scan-path reliability test has failed. This indicates that the JTAG controller and its cable cannot reliably communicate with the target system using that feature or algorithm. Try using the legacy frequency or a known good specific frequency. (Emulation package 5.0.872.0)

确定不是程序问题(在另一个板卡上可以运行),可能是硬件在航空托运中收到了损坏。感觉是JTAG时钟坏了