Part Number: TIDA-01580
Other Parts Discussed in Thread: LAUNCHXL-CC2640R2
将官网上下载的TIDA-01580-firmware按照手册分别烧写到CC2640R2 Development Kit和TIDA-01580-E2中,使用TIDA-01580 Application检测不到蓝牙连接,相应版本的labView已正确安装。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01580
Other Parts Discussed in Thread: LAUNCHXL-CC2640R2
将官网上下载的TIDA-01580-firmware按照手册分别烧写到CC2640R2 Development Kit和TIDA-01580-E2中,使用TIDA-01580 Application检测不到蓝牙连接,相应版本的labView已正确安装。
TIDA-01580-Application显示内容
CCS Base Folder
C:\ti\ccsv7\ccs_base
Project ,out file path
C:\Program Files(x86)\Texas Instruments\TIDA-01580\TIDA-01580_firmware\TIDA-01580_firmware_rx\FlashROM_StackLibrary\TIDA-01580_firmware_rx.out
Start/Stop
Stop
Status
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
CCS.lvlib:Open Port.vi->TIDA-01580 Application.vi中的打开TCB连接
Check if the Launchpad is connected properly
Check if .out is in the correct location
CCS版本为7.2.0 ,SDK版本号 simplelink_cc2640r2_sdk_1_40_00_45,使用手机端ble调试助手可找到对应的两个蓝牙设备