Part Number: TIDA-01606

这个芯片的2脚AINP和3脚AINN输入的是电流采样电阻的两端电压,但它分别对地电压都很高呀,为什么不会烧坏呢(虽然串了105电阻但没有对地电阻分压),如果电压被齐纳管钳位在5V+齐纳管压降后,那AINP和AINN的电压不就一样了,它还如何实现交流电压采样呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01606

这个芯片的2脚AINP和3脚AINN输入的是电流采样电阻的两端电压,但它分别对地电压都很高呀,为什么不会烧坏呢(虽然串了105电阻但没有对地电阻分压),如果电压被齐纳管钳位在5V+齐纳管压降后,那AINP和AINN的电压不就一样了,它还如何实现交流电压采样呢?
您好对于AMC1306的pin2和pin3来说,满足它的输入要求就好,您这里指的对地电压都很高,只要没超过AVDD就可以,参考它的电气参数:

哦,明白了,它这个AINN连接在AGND上,AGND又是浮动的。
AINP和AINN都是参考的AGND。 右边数字信号参考的是DGND。没有问题啊。