安装PSPICE-FOR-TI仿真软件时出现下图所示错误,请TI的老师帮忙分析下原因,谢谢。

cdsPspiceTIlog.txt日志如下
20:55:09 2022年1月20日 : parameter count = 1
20:55:09 2022年1月20日 : -wrapper
20:55:09 2022年1月20日 : Initializing
20:55:09 2022年1月20日 : Downloading URLs file from : pcb.cadence.com/.../TI_URLs.txt
20:55:11 2022年1月20日 : Response Content length = 1724
20:55:11 2022年1月20日 : C:\Users\Administrator\AppData\Roaming\Cadence\PspiceTIInstall\TI_URLs.txt bytes downloaded = 1724
20:55:11 2022年1月20日 : Reading Json URL File
20:55:11 2022年1月20日 : setting media download server URL from Json File
20:55:11 2022年1月20日 : Reading Json URL File
20:55:11 2022年1月20日 : setting Dll path from Json File
20:55:11 2022年1月20日 : Chws URL is: cdsplicwc.cadence.com/.../v1
20:55:11 2022年1月20日 : DownloadServerPath is: software-dl.ti.com/.../installer
20:55:12 2022年1月20日 : parameter count = 1
20:55:12 2022年1月20日 : -wrapper
20:55:13 2022年1月20日 : ReleaseVersion in XML: 17.40.007 InstalledVersion on system:
20:56:04 2022年1月20日 : An exception occured which is causing the program to close.
20:56:04 2022年1月20日 : Details of exception are : 无法加载 DLL“cdsVbl.dll”: 找不到指定的程序。 (异常来自 HRESULT:0x8007007F)。
20:56:04 2022年1月20日 : Stack Trace for the exception is 在 TIPSpice.Utilities.cdsVblRegisterInstallation(String productKey, String bundleName, String chwsUrl)
在 TIPSpice.Utilities.RegisterInstallation(String ProdKey)
在 TIPSpice.AuthWindow.AuthenticateUser()
在 System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
在 System.Windows.UIElement.RaiseEventImpl(DependencyObject sender, RoutedEventArgs args)
在 System.Windows.Controls.Primitives.ButtonBase.OnClick()
在 System.Windows.Controls.Button.OnClick()
在 System.Windows.Controls.Primitives.ButtonBase.OnMouseLeftButtonUp(MouseButtonEventArgs e)
在 System.Windows.RoutedEventArgs.InvokeHandler(Delegate handler, Object target)
在 System.Windows.RoutedEventHandlerInfo.InvokeHandler(Object target, RoutedEventArgs routedEventArgs)
在 System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
在 System.Windows.UIElement.ReRaiseEventAs(DependencyObject sender, RoutedEventArgs args, RoutedEvent newEvent)
在 System.Windows.UIElement.OnMouseUpThunk(Object sender, MouseButtonEventArgs e)
在 System.Windows.RoutedEventArgs.InvokeHandler(Delegate handler, Object target)
在 System.Windows.RoutedEventHandlerInfo.InvokeHandler(Object target, RoutedEventArgs routedEventArgs)
在 System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
在 System.Windows.UIElement.RaiseEventImpl(DependencyObject sender, RoutedEventArgs args)
在 System.Windows.UIElement.RaiseTrustedEvent(RoutedEventArgs args)
在 System.Windows.Input.InputManager.ProcessStagingArea()
在 System.Windows.Input.InputManager.ProcessInput(InputEventArgs input)
在 System.Windows.Input.InputProviderSite.ReportInput(InputReport inputReport)
在 System.Windows.Interop.HwndMouseInputProvider.ReportInput(IntPtr hwnd, InputMode mode, Int32 timestamp, RawMouseActions actions, Int32 x, Int32 y, Int32 wheel)
在 System.Windows.Interop.HwndMouseInputProvider.FilterMessage(IntPtr hwnd, WindowMessage msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
在 System.Windows.Interop.HwndSource.InputFilterMessage(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
在 MS.Win32.HwndWrapper.WndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
在 MS.Win32.HwndSubclass.DispatcherCallbackOperation(Object o)
在 System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)
在 System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)
在 System.Windows.Threading.Dispatcher.LegacyInvokeImpl(DispatcherPriority priority, TimeSpan timeout, Delegate method, Object args, Int32 numArgs)
在 MS.Win32.HwndSubclass.SubclassWndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam)
在 MS.Win32.UnsafeNativeMethods.DispatchMessage(MSG& msg)
在 System.Windows.Threading.Dispatcher.PushFrameImpl(DispatcherFrame frame)
在 System.Windows.Application.RunDispatcher(Object ignore)
在 System.Windows.Application.RunInternal(Window window)
在 TIPSpice.App.Main()
20:56:04 2022年1月20日 : Message: An error occurred and PSpice for TI needs to close.
Refer to cdsPspiceTIlog.txt at C:\Users\Administrator\AppData\Roaming\Cadence\PspiceTIInstall for error details.