This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

与DS90UB948控制断开

Part Number: DS90UB949A-Q1

Hi,

    1.硬件架构:DS90UB949A----(2-lane twisted STP)-----DS90ub948----(dual-link LVDS)-----TFT LCD(1920x720)

    2.实验现象:

      (1)通过DS90UB949A输出测试图案1920x720@60Hz,LCD是有正常的显示的,读写控制DS90UB948正常

        (2)   通过主机输出HDMI视频流给DS90UB949A,频率90MHz(REG[0x5F]读取值)后,与DS90UB948的控制通讯正常

        (3)   通过主机输出HDMI视频流给DS90UB949A,频率118.8MHz(REG[0x5F]读取值)后,与DS90UB948的控制通讯丢失,无法再读写DS90UB948。

        其他寄存器值 DS90UB949A的REG[0x5A]=0xCD, DS90UB948的REG[0x1C]=0x3B,2-lane twisted STP应该是正确的。

问题:

      (1)看DS90UB949A数据手册,2-lane模式下TMDS时钟应该是50~210MHz,1-lane模式TMDS时钟最大是105MHz?这个值是否就是REG[0x5F]的值?

        (2)  可否帮忙分析一下故障原因,建议一下后续的调试分析方法?