需求:-0~-15V可调节的10A电流的负压输出;
可调我可以用DAC调节,以前都是用BUCK改的,这次电流比较大,没有合适的芯片,请帮忙选一下谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需求:-0~-15V可调节的10A电流的负压输出;
可调我可以用DAC调节,以前都是用BUCK改的,这次电流比较大,没有合适的芯片,请帮忙选一下谢谢
Hi
还是建议用外部MOS的同步buck芯片来做,只是你输出电压从0V开始,需要外部运放调整一下。
具体选择多大电流的buck芯片,需要知道你的输入电压。
输入电压是24V,能推荐一下芯片吗?需要外部运放调整一下这个有没有参考设计?
Hi
输出超过39V, 电流能力大于10/ (1- 15/39)=16.25A的降压芯片都是可以的。
HI
输入
即你设计的输入电压加上输出电压绝对值: 24V+15V