This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高压信号发生器

超声激励电源模块技术要求:(二档180、500,或四档180、300、400、500)

(1)用途:激励5M的超声探头

(2)激励电压:180(不高于10%过冲)、500V(10%过冲,可略微放宽),2A驱动能力。

(3)激励频率:可调,最高8M(实际激励5M,要求频率稳定,希望有一定的余量)

(4)激励方式:脉冲个数、宽度可调,占空比50%

(5)输入电压:12V或24V

(6)输出阻抗不大于50Ω。

(7)脉冲重复频率:0-5KHz

请推荐控制芯片和成熟的方案!