This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pspice for TI

I have installed Pspice for TI software normally, and there were no errors during the installation process. The following prompt appears when running the program and creating the project file, as shown in the attached figure. Follow the prompts to run 'PspiceExplorerSrvr/regserver' without any response. May I ask how to handle this issue.
ERROR(ORCAP-1031): The OrCAD installation did not complete successfully. Cannot proceed.
To rectify this error, close Capture, run the following command by using the Start - Run menu option from the taskbar and restart Capture:
«installed path>\\tools\\bin\\Pspiceexplorersvr.exe/regserver
This is a prompt message