Other Parts Discussed in Thread: TINA-TI
计划将-9V电源的正极接入TPS43060的AGND与PGND记为SYS_GND,将负极接地并且接入TPS43060的输入端VIN,通过TPS43060将电压由输入的相对于SYS_GND的+9v压差升至输出的相对于SYS_GND为+12.3V的压差,以此获得相对于RS232的GND的3.3V压差
但在PSPICE仿真时,输入按如上所示接入TPS43060时芯片似乎没有正常工作,但使用+9V电源时芯片工作正常,对于TPS43060来说不论是+9V电源还是-9V电源,最后输入它的VIN-AGND不都是9V吗?为何会得到两种结果?在TINA-TI仿真也是同样的问题