Other Parts Discussed in Thread: LM76005,
使用官方下载的LM76005-Q1模型和仿真示例,修改了电路参数,实现48V转45.2V/4.5A,pspice for TI仿真LM76005的startup是正常的,但是将电路参数放到steadystate的示例中,仿真波形不正确。另外steadystate示例中的一个参数VOUTIC,我不太理解含义,我将其设置为45.2,不知道是否正确,其对steadystate仿真有什么影响吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用官方下载的LM76005-Q1模型和仿真示例,修改了电路参数,实现48V转45.2V/4.5A,pspice for TI仿真LM76005的startup是正常的,但是将电路参数放到steadystate的示例中,仿真波形不正确。另外steadystate示例中的一个参数VOUTIC,我不太理解含义,我将其设置为45.2,不知道是否正确,其对steadystate仿真有什么影响吗?
您好
针对这颗芯片,TI提供的是瞬态模型,没有提供稳态模型。如果进行steady state,可以按照下方链接的建议尝试一下,下方链接的情况和您的是一样的。
您是DC输入,VOUTIC指的是输出电压