您好,我目前在使用ADS1261EVM进行测试,需要屏蔽评估板自带的MCU而使用自己的MCU,目前我所知道的是需要对JP1进行连接来屏蔽,而其他的是需要将J6上的这些链接到自己的MCU上吗?我链接之后使用SPI无法读取数据。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我目前在使用ADS1261EVM进行测试,需要屏蔽评估板自带的MCU而使用自己的MCU,目前我所知道的是需要对JP1进行连接来屏蔽,而其他的是需要将J6上的这些链接到自己的MCU上吗?我链接之后使用SPI无法读取数据。
您好,
是的,请参考评估板用户手册“Schematic Block Diagram”
J6接口上的信号与外部MCU接口连接,包括给ADC的供电,SPI接口为图示红框部分。
ADS1261 and ADS1235 Evaluation Module User's Guide (Rev. A)
在芯片产品网页上有驱动代码,请参考。