This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51635: Power Designer問題

Part Number: LMR51635


Synchronous, Buck Converter,型號: LMR51635YDDCR,我想用power designer來用這個IC來設計電路,有碰到以下問題:

1. 在Configuration Options,由於這個IC是PFM模式,但是在ModeSetting裡面,沒有PFM模式,只有Auto Mode與FPWM模式可以選擇。

2. 在Frequency Selection裡面,我選1.1MHz,但是會系統會跳出"Design update failed - Max junction temperature exceeded",而且,當我調高設計條件的環境溫度的時候,最高沒辦法調超過50度,但是括號選項可以調整的範圍為(-40 - 125)。

以上問題再麻煩協助解決,謝謝。