Part Number: TPS40210
Other Parts Discussed in Thread: TINA-TI
TPS40210仿真无法启动
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
已经收到了您的案例,调查需要些时间,感谢您的耐心等待。
这是我的仿真原理图,仿真后输出一直等于输入电压28.我是用webench设计的输入28V-输出48V,1.3A电流。webench仿真没问题。我想在TINA-TI里添加我用的实际器件仿真,但是输出一直是28V,应该是TPS40210没有启动,请您帮我分析一下原因,谢谢。
示意图看起来不错。
请检查所有信号,如COMP引脚是否为高电平,BP引脚是否为高电平,DIS_EN_N是否为低电平。你能帮我计算一下你运行的模拟时间吗?因为信号需要时间才能上升。因此,请运行更长时间进行检查。
模拟仅运行2ms。
这段时间不足以看到设备的完全软启动。
SS上限为22nF。如果你把探针放在SS引脚上,你应该看到电压在这2ms内已经上升了。然而,由于您的Vout已经预偏置到28V的输入电压,因此设备只有在软启动参考电压达到该水平时才会开始切换。
如果你想减少模拟时间,只想检查模拟模型是否正在运行,你可以将SS上限设置为100pF以“禁用”软启动。
您还可以保留22nF并增加模拟时间。我建议将时间定在30毫秒以上,以实现全面提升。