This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23: Why can't I run a simulation with this IC?

Part Number: TPS546C23


Dear customer support center,

I would like to use the TPS546C23 for simulation design, but the system says the design cannot be created. Could you please let me know why this is happening?

The design conditions are as follows:

1. Input Vin min: 11V, Vin max: 13V, Vin nominal: 12V

2. Output: 0.875V, Iout max: 35A, Iout nominal: 15V, Vout max ripple: 2%

3. Design Consideration: balanced

Please assist with the response. Thank you.