This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2540的pairing问题



基于官方1.4.1协议栈,部分代码如下:

uint32 passkey = 1234; // passkey "000000"
uint8 pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8 mitm = TRUE;
uint8 ioCap = GAPBOND_IO_CAP_DISPLAY_YES_NO;
uint8 bonding = FALSE;

static void ProcessPasscodeCB(uint8 *deviceAddr,uint16 connectionHandle,uint8 uiInputs,uint8 uiOutputs )
{
uint32 passcode = 1234;

// Send passcode response
GAPBondMgr_PasscodeRsp( connectionHandle, SUCCESS, passcode );
}

用这样的配置, 然后用iPhone连接,出现这样的情况:手机弹出输入密码,但是我按了取消,然后照样是显示“连接成功”。 这是怎么回事!?