This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1:信道探测打印结果data解析

Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: CC2745P10-Q1

您好 这是我使用LP-EM-CC2745R10-Q1开发板进行信道探测的输出结果,使用的sdk是simplelink_lowpower_f3_sdk_9_12_00_19,我在选择输出raw_events时输出了如下的数据,请问输出的data是什么,是未经过滤的IQdata吗,并且我想知道有没有具体的数据(就是下文的data)解析的格式,就比如02:13:09:00:2B:52:E6:04:42:12:07:0C这12个字节都代表了什么

Waiting for CS_SUBEVENT_RESULTS (local)
Subevent Results - local device
----------------------------------------------------------------------
_io: []
event: 69
conn_handle: 0
config_id: 0
start_acl_connection_event: 288
procedure_counter: 0
frequency_compensation: 0
reference_power_level: -51
procedure_done_status: 1
subevent_done_status: 1
abort_reason: 0
num_antenna_path: 1
num_steps_reported: 20
data_len: 228
data: 00:48:05:02:7F:01:00:C0:00:27:05:02:7F:01:00:C0:00:2F:05:02:7F:01:00:C0:02:10:09:00:E5:9F:00:24:F8:3F:01:26:02:27:09:00:F6:7F:FF:2C:FB:BF:FF:2E:02:20:09:00:00:90:FF:1E:00:E0:FF:28:02:23:09:00:FF:0F:00:89:00:20:00:82:02:1E:09:00:04:F0:FF:58:04:F0:FF:85:02:48:09:00:04:A0:FF:8C:04:A0:FF:74:02:49:09:00:02:A0:FF:78:03:90:FF:53:02:09:09:00:FB:1F:00:55:FB:0F:00:64:02:32:09:00:03:C0:FF:A6:03:C0:FF:64:02:3B:09:00:FC:DF:FF:C8:FC:BF:FF:AF:02:06:09:00:FC:1F:00:8E:FB:0F:00:7D:02:3C:09:00:03:D0:FF:85:04:D0:FF:74:02:36:09:00:00:C0:FF:C8:FF:CF:FF:C8:02:05:09:00:FD:FF:FF:96:FB:1F:00:96:02:22:09:00:00:00:00:85:FF:0F:00:A6:02:35:09:00:FF:AF:FF:64:00:C0:FF:C8:02:15:09:00:05:20:00:78:00:00:00:C8
----------------------------------------------------------------------
Waiting for CS_SUBEVENT_RESULTS (remote)
Subevent Results - remote device
----------------------------------------------------------------------
_io: []
event: 69
conn_handle: 0
config_id: 0
start_acl_connection_event: 288
procedure_counter: 0
frequency_compensation: -16384
reference_power_level: -51
procedure_done_status: 1
subevent_done_status: 1
abort_reason: 0
num_antenna_path: 1
num_steps_reported: 21
data_len: 234
data: 00:48:03:02:7F:01:00:27:03:02:7F:01:00:2F:03:02:7F:01:02:10:09:00:00:00:00:FA:01:D0:FF:FA:02:27:09:00:09:30:00:68:03:10:00:75:02:20:09:00:08:B0:00:25:01:80:00:1A:02:23:09:00:01:F0:FF:A0:FF:0F:00:8D:02:1E:09:00:02:E0:FF:8C:00:00:00:96:02:48:09:00:FF:CF:FF:96:00:C0:FF:C8:02:49:09:00:00:D0:FF:FF:00:D0:FF:A6:02:09:09:00:F8:BF:FF:3F:F9:AF:FF:3F:02:32:09:00:02:C0:FF:85:01:B0:FF:7D:02:3B:09:00:FE:EF:FF:96:FF:FF:FF:FA:02:06:09:00:FE:CF:FF:2E:FC:CF:FF:38:02:3C:09:00:04:D0:FF:96:03:C0:FF:B4:02:36:09:00:FF:CF:FF:85:FF:CF:FF:C8:02:05:09:00:FB:EF:FF:35:FC:CF:FF:2E:02:22:09:00:00:00:00:FA:01:00:00:64:02:35:09:00:FF:DF:FF:64:FE:DF:FF:C8:02:15:09:00:FF:CF:FF:96:FF:DF:FF:FF:02:14:09:00:FD:8F:FF:3A:02:00:00:FF

  • 首先,请使用 9.11.01.19 版本,该版本包含针对通道测量的最新开发和错误修复。我们将很快更新 SDK 页面,内容如下:

    Note:

    - LPF3 9.11.01.19 is intended for Bluetooth LE car access users who are developing with the latest Channel Sounding updates. It does not have production CC27xxP10 device support.

    - LPF3 9.12.01.19 is the Production-ready release for CC2745P10-Q1 including final characterized RF settings. It does not have Bluetooth LE car access/CS updates.

    - Full support for both features mentioned above will be provided in a future SDK.

    其次,您提出的上述问题似乎与以下问题完全相同。如果是这样,请避免重复发布相同的问题,以便我们可以限制重复工作。

    e2echina.ti.com/.../cc2745r10-q1-channel-sounding-subevent-results