硬體: cc2541+cc2591
使用一段時間後(1小時內~12小時以上都有遇過),
發現sniffer和手機都掃描不到cc2541,
當cc2541停止廣播時,
用Debugger查看gapRoleState是GAPROLE_ADVERTISING
此時卻可以用長按按鈕來觸發LED閃爍(做法是中斷+osal timer)
reset或者斷電重啟後, 即可恢復廣播
廣播相關的代碼如下,
#define DEFAULT_ADVERTISING_INTERVAL_MIN 32 // 20ms
#define DEFAULT_ADVERTISING_INTERVAL_MAX 48 // 30ms
#define DEFAULT_DISCOVERABLE_MODE GAP_ADTYPE_FLAGS_GENERAL
{
// For other hardware platforms, device starts advertising upon initialization
uint8 initial_advertising_enable = TRUE;
// By setting this to zero, the device will go into the waiting state after
// being discoverable for 30.72 second, and will not being advertising again
// until the enabler is set back to TRUE
uint16 gapRole_AdvertOffTime = 0;
}
// Set advertising interval
{
uint16 advIntMin = DEFAULT_ADVERTISING_INTERVAL_MIN;
uint16 advIntMax = DEFAULT_ADVERTISING_INTERVAL_MAX;
// GAP_SetParamValue( TGAP_LIM_DISC_ADV_INT_MIN, advInt );
// GAP_SetParamValue( TGAP_LIM_DISC_ADV_INT_MAX, advInt );
GAP_SetParamValue( TGAP_GEN_DISC_ADV_INT_MIN, advIntMin );
GAP_SetParamValue( TGAP_GEN_DISC_ADV_INT_MAX, advIntMax );
}
閃爍的做法是用osal timer 如下
uint16 SimpleBLEPeripheral_ProcessEvent( uint8 task_id, uint16 events )
{
// ...
if ( events & LED_BLINKING_EVT )
{
LED_PIN = ~LED_PIN; // 切換LED狀態
counter_led++;
if ( counter_led < led_blink_times )
{ // restart led blinking timer
osal_start_timerEx( simpleBLEPeripheral_TaskID, LED_BLINKING_EVT, LED_BLINKING_PERIOD );
}
return (events ^ LED_BLINKING_EVT);
}
}
請問為什麼會停止廣播呢?