This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2540进不去低功耗的问题

Other Parts Discussed in Thread: CC2540

我在CC2540从机程序中,已经开启了POWER_SAVING,也能进osal_pwrmgr_powerconserve(),但是发现pwrmgr_attribute.pwrmgr_task_state==2,功耗测下来是8mA,连PM2都没进去,Debug发现osal_run_system()一直在跑,我关掉了所有的自己设置的定时事件,感觉还是有任务在跑,可又找不到,TI的技术人员能不能帮帮忙给个解决思路

  • yang,

    你用的是TI的EVM板吗?如果不是,你的程序能在TI的EVM板上试试看吗?

    照理论上说,只要没有连接,没有任何定时事件,系统就会进入PM3, 有timer或者连接的情况下会进入PM2。

    你有修改去手动调用 osal_pwrmgr_powerconserve() 吗?如果这样做了,建议你用默认的程序试试看。

  • Y,你好

    我用的是TI原厂的板子,没有修改和手动调用osal_pwrmgr_powerconserve() 这个函数。经过下午查资料和调试,我在宏定义加入了HAL_UART_DMA=0,pwrmgr_attribute.pwrmgr_task_state可以等于0了,问题是

    void osal_pwrmgr_powerconserve( void )
    {
      uint32        next;
      halIntState_t intState;

      // Should we even look into power conservation
      if ( pwrmgr_attribute.pwrmgr_device != PWRMGR_ALWAYS_ON )
      {
        // Are all tasks in agreement to conserve
        if ( pwrmgr_attribute.pwrmgr_task_state == 0 )
        {
          // Hold off interrupts.
          HAL_ENTER_CRITICAL_SECTION( intState );

          // Get next time-out
          next = osal_next_timeout();

          // Re-enable interrupts.
          HAL_EXIT_CRITICAL_SECTION( intState );

          // Put the processor into sleep mode
          OSAL_SET_CPU_INTO_SLEEP( next );
        }
      }
    }

    我在debug里面看到,它会不断地进入if ( pwrmgr_attribute.pwrmgr_task_state == 0 )这个判断语句,按理说进入一次就可以了,就好像有一个东西在不断的唤醒,而我查不出来。