This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: 如何读取UART接收溢出错误和重新使能UART接收

Part Number: CC2340R5

CC2340R5,SDK V912

当UART发生接收溢出错误OE,UART ROM API会自动禁止接收。如何能获取UART接收溢出错误,并重新使能接收?如下是目前使用的获取方法

1、当发生OE错误时,并没有停在设置断点处,而观察UART寄存器指示溢出

uartParams.readMode = UART2_Mode_CALLBACK;
uartParams.writeMode = UART2_Mode_CALLBACK;
uartParams.readCallback = uartReadCallback;

static void uartReadCallback(UART2_Handle handle, void *rxBuf, size_t size, void *userArg, int_fast16_t status)
{

  if (status != UART2_STATUS_SUCCESS)
  {
    /* RX error occured in UART2_read() */
    __NOP();                                                        //这里设置断点
  }

  uartMessageLength = (uint16)(size);
  BLEAppUtil_invokeFunctionNoData(sendDataOverBLE); //+++ Crucial to call from task and not interrupt context, otherwise the application aborts and crashes
}