Part Number: CC23XX-REPORTS
Other Parts Discussed in Thread: CC2745R10-Q1
- 环境
- SWD Test Connection 执行正常
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\26300996\AppData\Local\TEXASI~1\
CCS\ccs1271\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Apr 19 2024'.
The library build time was '14:04:01'.
The library package version is '12.7.0.00130'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller to enter SWD mode.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the SWD Mode Integrity test]-----------------------------------
This test will read the IDCODE register 1 time.
The IDCODE register value is 0x6ba02477.
The SWD Mode Integrity test has succeeded.
[End: Texas Instruments XDS110 USB Debug Probe]
3. 仿真下载报错,如下图