This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1: channel sounding compensation frequency

Part Number: CC2745R10-Q1

我目前在使用cc2745R10-Q1进行信道探测任务时,我们注意到在输出输出中,有一个compensation frequency参数 这个参数的量总是在32000上下浮动,我想请问这个compensation frequency具体代表了什么意思呢,他在remote设备和local设备进行距离估计时,起到了哪些作用?

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 您好,

         根据 BLE 规范,补偿频率被定义为“parameter indicates the value of the fractional frequency offset (FFO) used by the initiator device to align the timing of CS steps and transmit frequencies during non-mode-0 CS steps”。

    本质上,补偿频率用于在整个信道测量过程中保持频率时序一致,以考虑来自其他源的变化和干扰。