Other Parts Discussed in Thread: TPS62730, CC2541, CC2540
我把ANCS集成到KeyFob里了,添加了两个task,分别是处理KeyFob和Ancs的任务
/* Application */
KeyFobApp_Init( taskID++ );
TimeApp_Init(taskID);
并在初始化的时候通过调用GATT_RegisterForInd注册了ancs的task做为接收task,现在的问题是与手机上的APP连接上(Keyfob里的服务和ANCS都连接上,功能也正常),然后把APP杀掉,但ANCS也不会断开,于是设备端不知道KeyFob里的服务断开了,不能继续广播,于是再打开APP就搜索不到设备了,我要怎么获取KeyFob里的服务是否断开了?断开后我要重新广播。
两个task的init函数如下 :
void TimeApp_Init( uint8 task_id )
{
timeAppTaskId = task_id;
// Register to receive incoming ATT Indications/Notifications
GATT_RegisterForInd( timeAppTaskId );
// Setup a delayed profile startup
osal_set_event( timeAppTaskId, START_DEVICE_EVT );
}
oid KeyFobApp_Init( uint8 task_id )
{
keyfobapp_TaskID = task_id;
// Setup the GAP
VOID GAP_SetParamValue( TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL );
// Setup the GAP Peripheral Role Profile
{
// For the CC2540DK-MINI keyfob, device doesn't start advertising until button is pressed
uint8 initial_advertising_enable = FALSE;
// By setting this to zero, the device will go into the waiting state after
// being discoverable for 30.72 second, and will not being advertising again
// until the enabler is set back to TRUE
uint16 gapRole_AdvertOffTime = 0;
uint8 enable_update_request = DEFAULT_ENABLE_UPDATE_REQUEST;
uint16 desired_min_interval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
uint16 desired_max_interval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
uint16 desired_slave_latency = DEFAULT_DESIRED_SLAVE_LATENCY;
uint16 desired_conn_timeout = DEFAULT_DESIRED_CONN_TIMEOUT;
// Set the GAP Role Parameters
GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8 ), &initial_advertising_enable );
GAPRole_SetParameter( GAPROLE_ADVERT_OFF_TIME, sizeof( uint16 ), &gapRole_AdvertOffTime );
GAPRole_SetParameter( GAPROLE_SCAN_RSP_DATA, sizeof ( deviceName ), deviceName );
GAPRole_SetParameter( GAPROLE_ADVERT_DATA, sizeof( advertData ), advertData );
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );
GAPRole_SetParameter( GAPROLE_MIN_CONN_INTERVAL, sizeof( uint16 ), &desired_min_interval );
GAPRole_SetParameter( GAPROLE_MAX_CONN_INTERVAL, sizeof( uint16 ), &desired_max_interval );
GAPRole_SetParameter( GAPROLE_SLAVE_LATENCY, sizeof( uint16 ), &desired_slave_latency );
GAPRole_SetParameter( GAPROLE_TIMEOUT_MULTIPLIER, sizeof( uint16 ), &desired_conn_timeout );
}
// Set the GAP Attributes
GGS_SetParameter( GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, attDeviceName );
// Setup the GAP Bond Manager
{
uint32 passkey = DEFAULT_PASSCODE;
uint8 pairMode = DEFAULT_PAIRING_MODE;
uint8 mitm = DEFAULT_MITM_MODE;
uint8 ioCap = DEFAULT_IO_CAPABILITIES;
uint8 bonding = DEFAULT_BONDING_MODE;
GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof( uint32 ), &passkey );
GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof( uint8 ), &pairMode );
GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof( uint8 ), &mitm );
GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof( uint8 ), &ioCap );
GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof( uint8 ), &bonding );
}
// Initialize GATT Client
VOID GATT_InitClient();
// Initialize GATT attributes
GGS_AddService( GATT_ALL_SERVICES ); // GAP
GATTServApp_AddService( GATT_ALL_SERVICES ); // GATT attributes
DevInfo_AddService(); // Device Information Service
ProxReporter_AddService( GATT_ALL_SERVICES ); // Proximity Reporter Profile
Batt_AddService( ); // Battery Service
Accel_AddService( GATT_ALL_SERVICES ); // Accelerometer Profile
SK_AddService( GATT_ALL_SERVICES ); // Simple Keys Profile
keyfobProximityState = KEYFOB_PROXSTATE_INITIALIZED;
// Initialize Tx Power Level characteristic in Proximity Reporter
{
int8 initialTxPowerLevel = 0;
ProxReporter_SetParameter( PP_TX_POWER_LEVEL, sizeof ( int8 ), &initialTxPowerLevel );
}
keyfobAlertState = ALERT_STATE_OFF;
// make sure buzzer is off
buzzerStop();
// makes sure LEDs are off
HalLedSet( (HAL_LED_1 | HAL_LED_2), HAL_LED_MODE_OFF );
// For keyfob board set GPIO pins into a power-optimized state
// Note that there is still some leakage current from the buzzer,
// accelerometer, LEDs, and buttons on the PCB.
P0SEL = 0; // Configure Port 0 as GPIO
P1SEL = 0x40; // Configure Port 1 as GPIO, except P1.6 for peripheral function for buzzer
P2SEL = 0; // Configure Port 2 as GPIO
P0DIR = 0xFC; // Port 0 pins P0.0 and P0.1 as input (buttons),
// all others (P0.2-P0.7) as output
P1DIR = 0xFF; // All port 1 pins (P1.0-P1.7) as output
P2DIR = 0x1F; // All port 1 pins (P2.0-P2.4) as output
P0 = 0x03; // All pins on port 0 to low except for P0.0 and P0.1 (buttons)
P1 = 0; // All pins on port 1 to low
P2 = 0; // All pins on port 2 to low
// initialize the ADC for battery reads
HalAdcInit();
// Register for all key events - This app will handle all key events
RegisterForKeys( keyfobapp_TaskID );
#if defined ( DC_DC_P0_7 )
// Enable stack to toggle bypass control on TPS62730 (DC/DC converter)
HCI_EXT_MapPmIoPortCmd( HCI_EXT_PM_IO_PORT_P0, HCI_EXT_PM_IO_PORT_PIN7 );
#endif // defined ( DC_DC_P0_7 )
// Setup a delayed profile startup
osal_start_timerEx( keyfobapp_TaskID, KFD_START_DEVICE_EVT, STARTDELAY );
}