This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540的Timer1寄存器问题

Other Parts Discussed in Thread: CC2540

目前有个项目用到CC2540使用OSAL蓝牙栈,项目应用中使用Timer1作为PWM输出的计数器,使用center-aglin,同时开启Timer1中断,使用中断对PWM输出的个数进行计算;发现中断计数的个数与实际不符,理论上计数个数应该为实际输出个数的2倍;断点后查看,发现中断中T1STAT的中断源无法清除,且中断源的mask bit对T1STAT的中断源没有控制;项目实际应用ch1和ch2,已经屏蔽ch0.2.3.4和T1的overflow的mask bit;中断查看是还是T1STAT的ch2还是被置位。代码如下,请达人或TI的员工能给一个答复。谢谢!

 /*
*  函数名:ini_pwm
*  函数功能: 初始化并启动pwm 输出
*  参数: aa 要产生的2微秒延时个数
*/
void ini_pwm() //初始化PWM相关寄存器
{
  CC_TYPE unTicks;  //装载到T1CC0寄存器中的数据
  uint8 u8TickSpdDiv;  //取得时钟的前期分频CLKCONSTA.TICKSPD的值
//disable interrupt mask bit
T1CCTL0 &= ~0xC0; //disable RF and channel 0 interrupt mask bit
T1CCTL1 &= ~0x80; //disable RF interrupt mask bit
T1CCTL2 &= ~0xC0; //disable RF and channel 2 interrupt mask bit
T1CCTL3 &= ~0xC0; //disable RF and channel 3 interrupt mask bit
T1CCTL4 &= ~0xC0; //disable RF and channel 4 interrupt mask bit
TIMIF   &= ~0x40; //disable Timer1 overflow interrupt mask bit

  
  CLKCONSTA = 0;
  u8TickSpdDiv = (CLKCONSTA & 0x38) >> 3; //获取当前定时器时钟源的预分频
  unTicks.u16Counters = ((MAIN_CLOCK / SEND_FRE) >> u8TickSpdDiv) / 2;  // 
  //由于我们的主时钟为32Mhz,要得到的频率为125Khz,并且定时器T1CTL.DIV=0,即预分频为0
  //因此就算是u8TickSpdDiv为0.我们得到的u16Ticks的最大值为32000000/125000=256
  
  
  
  T1CC0L = unTicks.u8Counters[0];   //PWM波周期设定
  T1CC0H = unTicks.u8Counters[1];
  
  unTicks.u16Counters = ((unTicks.u16Counters) * 55)/100;
  T1CC1L = unTicks.u8Counters[0];   //占空比设置,设定为50%占空比
  T1CC1H = unTicks.u8Counters[1];

  unTicks.u16Counters = ((MAIN_CLOCK / SEND_FRE) >> u8TickSpdDiv) / 2;
  unTicks.u16Counters = ((unTicks.u16Counters) * 45)/100;
  T1CC2L = unTicks.u8Counters[0];   //占空比设置,设定为50%占空比
  T1CC2H = unTicks.u8Counters[1];
  
  T1CCTL1 |= 0x04;           // 通道1设定为比较模式
  T1CCTL1 |= 0x18;           // 向上比较设置输出,在0清零
  
  T1CCTL2 |= 0x04;           // 通道1设定为比较模式 
  T1CCTL2 |= 0x20;           //向上比较清除输出,在0设置
                             //设置pwm输出模式,T1CCTL1和T1CCTL2的输出模式使得
                             //两路PWM波是对称输出的
PERCFG |= 0x40;            // 将timer1的端口移动到备用端口2
  P1SEL |= 0x03;             // P1_0 为pwm2口,P1_1为pwm1口
  P1DIR |= 0x03;             //p1_0,p1_0口为输出                             
  T1IE = 1;//使能T1IE 
  T1CTL |= UP_AND_DOWN_MODE;              //开启pwm工作使用从0到T1CC0反复计数
}

#pragma vector = T1_VECTOR                     
 __interrupt void T1_ISR(void) 
{  
if(T1STAT & 0x02)
{
T1STAT &= ~0x06;   // clear interrupt sourse bit
if(m_Cap.Sendpwm_Num > 0)
   {  
     m_Cap.Sendpwm_Num--; 
P0_4 = !P0_4;
   }
   else

T1CTL &= 0xFC;

}
  


//*********************************************
//函数名称:sendPWM
//
//输入参数:void
//
//输出参数:void
//
//功能描述:产生125Khz占空比为50%的PWM波
//修改历史:
//*********************************************
void sendPWM(void)

  ini_pwm();               //timer 1配置初始化 
#if 1  
  while(m_Cap.Sendpwm_Num !=0)
   {};
   STOP_PWM();



#else
  {
    delay(196);delay(196);delay(196);delay(196);delay(196);delay(196);
    delay(196);delay(196);delay(196);delay(196);delay(196);delay(196);
  } 
  STOP_PWM();                   //关闭pwm工作
 
#endif
}


//*********************************************
//函数名称:stopPWM
//
//输入参数:void
//
//输出参数:void
//
//功能描述:停止产生PWM波且输出为低
//修改历史:
//*********************************************
void STOP_PWM(void)
{
PERCFG |= 0x40;            // 将timer1的端口移动到备用端口2
P1SEL &= ~0x03;             // P1_0 为pwm2口,P1_1为pwm1口
  P1DIR |= 0x03;             //p1_0,p1_0口为输出
  P1    &= ~0x03;            //low
 
}