This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 STANDBY ISSUR



Dear  all,

        以下问题请教一下:

        设备工作状态如下:按0.5S的时间间隔进行广播模式。

        1)如果在3.7V电池供电情况下,可以手机APP和设备正常连接通信,断开之后设备也会进入上述模式,当然在非广播的情况下,是处于STANDBY的模式

        以上情况下 设备工作正常。

        2)现在换成3V的电池供电情况,但是出现情况,如果手机不连接APP的情况下,设备还是可以正常的工作,一旦手机APP连接,然后断开之后  整个设备已经无法进入正常的广播模式,从外面来看设备好像是死机一样。

        目前设备使用的是内部的DCDC模式,和例程一样的进行的POWER部分设计,因此对上述现象不是很理解,想看看有朋友遇到过这样的问题么,初步怀疑是电源的问题,但是从芯片的供电范围是1.8到3.7V 因此不应该。