测试发现Inquiry时的电流为40mA,大大超出我的预想。
我尝试用过VS_Set_Max_Output_Power这个函数,但是不起作用。
我还可以通过什么方法来降低电流呢?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测试发现Inquiry时的电流为40mA,大大超出我的预想。
我尝试用过VS_Set_Max_Output_Power这个函数,但是不起作用。
我还可以通过什么方法来降低电流呢?谢谢
我控制的Inquiry时间为1.28s,但是我还想控制inquiry电流。
使用VS_Set_Max_Output_Power 、HCI_Write_Inquiry_Transmit_Power_Level这两个都没有成功降低功耗
你测量的时候是整个1.28S都是40mA左右的功耗?还是只有一个峰峰值是这么多,inquiry的整个平均功耗不会这么高
PS:不建议通过降低output power的方法降低功耗,因为通信距离也同时降低了