TI工作人员您好,
我最近在用CC2541做一个蓝牙温湿度计的设计,系统中有温湿度,LCD和flash。现在固件和驱动都写好了,但是遇到一些蓝牙稳定性问题。
蓝牙模块工作几个小时后,手机就搜索不到蓝牙设备了,但是温湿度的数据还能正常读取,也能在LCD上实时的显示出来。看了flash的读写波形和时间间隔,也是和设计的效果一样。
请问你们有遇到类似的问题么,有什么解决办法或者需要排查的点么??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
是32768的晶振问题吗?
32768的晶振会影响到蓝牙连接问题。因为CC2541唤醒同步蓝牙是靠32768晶振来定时计算的。
在CC2541上,我们哟要求晶振必须符合下面的规范。
另外,你可以通过关闭power saving来一致使能CC254x设备来判断问题是否由32768晶振造成。
Manufacturer | MPN | Package | ESR [ohm] | CL [pF] | Tol [ppm] | Temp tol [ppm] | Aging [ppm/year] | Temp range [deg C] | Used in TI reference? | Tested by external lab? |
---|---|---|---|---|---|---|---|---|---|---|
NDK | NX2016SA 32MHz EXS00A-CS04859 | 2016 | 60 | 10 | +/- 15 | +/- 25 | -40 / +105 | Yes | - | |
NDK | NX3225SA 32MHz EXS00A-02994 | 3225 | 50 | 16 | +/- 10 | +/- 15 | -30 / +125 | Yes | - | |
Epson Toyocom | FA-128 | 2016 | 60 | 10 | +/- 10 | +/- 10 | 5 | -40 / +85 | Yes | - |
Epson Toyocom | FA-20H | 2520 | 60 | 10 | +/- 10 | +/- 10 | 3 | -40 / +85 | Yes | - |
NDK | NX3225GA 32 MHz EXS00A-CG02611 | 3225 | 50 | 10 | +/- 20 | +/- 20 | -40 / +85 | Yes | - | |
NDK | NX2016SA 32.000MHz EXS00A-CS05931 | 2016 | 60 | 10 | +/- 15 | +/- 25 | -40 / +125 | CC2540T BLE Light | - |
Manufacturer | MPN | Package | ESR max [ohm] | CL [pF] | Tol [ppm] | Temp tol [ppm] | Aging [ppm/year] | Temp range [deg C] | Used in TI reference? | Tested by external lab? |
---|---|---|---|---|---|---|---|---|---|---|
Epson Toyocom | FC-12M | 2012 | 90k | 12.5 | +/- 20 | 3 | -40 / +85 | Yes | - | |
Epson Toyocom | MC306 | 8.0 x 3.8 mm | 12.5 | 20 | +/- 50 | -40 / +85 | Yes | - | ||
NDK | NX3215SA 32.768KHz EXS00A-MU00109 | 3215 | 90k | 12.5 | +/- 20 | +/- 3 | -30 / +85 | No | - | |
NDK | NX3215SA 32.768KHz EXS00A-MU00301 | 3215 | 80k | 12.5 | +/- 20 | -40 / +125 | CC2540T BLE Light | - |