Other Parts Discussed in Thread: CC2541, CC2640
像下面的用于DTM测试的HCI命令一共有多少?可以通过这些HCI命令,使用CMW500来测试收发机的各项性能吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
1、附件里没找到这个命令HCI_LE_Transmitter_Test ?
2、如果使用CMW500来测试,我有一个SmartRF06EB+EM,是否使用软件smart RF studio控制,cable线接到CMW就可以进行收发机的各项测试?
3、以上测试应该算是非信令测试吧?BLE有信令测试的吗?如果有,怎么进行?
Q3; 综测仪应该即支持信令也支持非信令,可以咨询仪器厂商,如何进行。 CC26XX 按照DTM方式,打开了HCI接口,至于发什么测试命令是由测试仪决定的。
5、我频谱仪直接设置2.4GHz-2.5GHz的,smart RF studio7哪里设置ble mode?没有看到,continuous TX和packet TX在频谱仪上都看不到输出
6、已经解决,谢谢!