Other Parts Discussed in Thread: CC2592, CC2530, CC2538
Dear Sir,
RF input of CC2592 is balance architecture. Can it work in un-balance? If yes, how can it be performed. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alan,
It should work.
but I think the gain will be lower around 3dB if you terminate another port.
you can refer to Figure 5-1. CC2592 Evaluation Module, the EVM is tested based on an external Balun.
BR. Albin