CC2650支持蓝牙4.2吗??如果不支持,TI现在哪个芯片支持??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
支持的,
Q: Does CC2640 Support Bluetooth version 4.2 or Mesh Networks
The CC2640 with BLE-Stack v2.2.1 supports Bluetooth core specification version 4.2 including all new LE features (LE Secure Connections, LE Data Length Extension, LE Privacy 1.2). Additionally, support is provided for all Bluetooth version 4.1 core specification LE features, including multi Master/Slave capability ("MultiRole") for connections up to 8 devices. As with all LE features added after the initial Bluetooth 4.0 specification, support of v4.1 and v4.2 features are optional. The TI BLE-Stack allows you to selectively configure just the features (v4.0, v4.1 and v4.2) that are needed for your application.
A description for using the v4.2 features is provided in the included CC2640 BLE Software Developer’s Guide (SWRU393).
On November 11, 2015, the Bluetooth SIG announced enhancements to Bluetooth low energy coming in 2016, including official support for Mesh Networks. TI intends to support the SIG Mesh standard sometime after the official standard is adopted by SIG.
目前TI的BLE协议栈最新版本是BLE-STACK 2.2.1,它是支持Bluetooth 4.2的。目前官方给出的version是7.70.2
The following IDEs are supported by this SDK:
IDE |
Version |
Tool Chain |
Notes |
Code Composer Studio (CCS) |
6.2.0 (Build 50 or later) |
TI ARM Compiler v5.2.6 |
A free CCS v6 license is provided when used with a TI CC26xx or CC13xx development kit that includes an XDS100v3 or XDS110 debugger. Other compiler versions may not compatible with this SDK. Refer to Section 2.6.3 Code Composer Studio in the SWRU393_CC2640_BLE_Software_Developer’s_Guide for the procedure to install TI ARM Compiler version 5.2.6. |
IAR Embedded Workbench for ARM |
7.70.2 |
Included |
A time limited evaluation version may be available. Please note the fully functional (non size-limited) version of IAR is required. |
有些旧版本也是可以打开工程的,但还是建议您使用比较新的版本,因为更新及优化了一些特性