TI 工程师您好,请问CC2541芯片本身有BQB认证吗?如果有的话,认证证书可以提供吗? 谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
以下是认证人员对于该问题的回复:
-The Bluetooth Low Energy (BLE) (Smart Bluetooth / Bluetooth 4.0) is not compatible with the classic Bluetooth. It means that with a slave-mode BLE system can not communicate with a standard Bluetooth system.
-There are specific qualifications and steps to pass in order to be certified as Bluetooth Low Energy. Then since the BLE BT4.0 chip should be already certified with the Bluetooth 4.0 qualification body, you will only need a shorter-process for the certification of your final system (still including the Bluetooth 4.0 qualification body)
CC254X系列如果需要做其他认证, 请参考我们这边的文档: http://processors.wiki.ti.com/index.php/How_to_Certify_your_Bluetooth_product