This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564B同时连接BLE和HSP,BLE notify有延时



CC2564B作主机同时连接BLE和HSP两个从机设备,当CC2564B与HSP建立sco连接后,BLE notify有时候有延时(延时时间大概在500ms左右,延时要么一直都有,要么就没有,延时决定时刻在建立SCO连接时)。断开SCO连接,没有BLE的notify延时。到底是什么原因啊?

btsp是最新版v1.6,BLE的interval  8;

协议栈里面有没有设置BLE优先级的功能?我的notify数据很少,且频度低,但要求响应速度快,需要优先处理。

在BLE端,按键按下,就notify数据给CC2564B,CC2564B收到数据就立即通过串口打印出来,按键按下与打印出结果中间有时有明显的延时,不知道这样判断有延时是否可靠?还是串口打印函数本身有可能有延时?

  • 根据手册: The following technologies and assisted modes cannot be used simultaneously with the coprocessor: Bluetooth LE

    而HSP只能在assisted mode下使用,所以不能与BLE同时使用

  • Viki Shi 说:

    根据手册: The following technologies and assisted modes cannot be used simultaneously with the coprocessor: Bluetooth LE

    而HSP只能在assisted mode下使用,所以不能与BLE同时使用

    hi,Viki Shi

    The assisted modes (HFP 1.6 and A2DP) are not supported simultaneously. Furthermore, the assisted modes are not supported simultaneously with BLE or ANT.

    我的理解是assisted modes只包括HFP 1.6(WBS) 和A2DP,没有找到含有HSP的说明啊?所以我当时选择了HSP,不知道理解是否正确。

  • HSP也只能在assisted mode下使用